You are here: Technical References > Fieldbus Library > EtherCAT Library > EtherCAT Library - SDO

EtherCAT Library - SDO

These function blocks are used to work with drive or remote I/O parameters that are not supported by ML and MC function blocks.

DriveControl device for regulating the speed, torque and position of a motor or remote I/O parameters that have an associated SDO number can be read and written using these function blocks.

See also the FAQ to how to set up the update rate for SDO communication.

 

ECATReadSdo

ECATWriteSdo


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™